Change Language :
Design guidance & tips that make using igus® plastic machinery components easy in any application.
Welcome to TechTalk, a design advice series created and written by igus® product managers, which offers design guidance and tips that make specifying igus®' plastic machinery components simple in any application.
Index
linear bearings and guides
In this TechTalk article, learn how to eliminate binding and stick-slip in linear plastic bearings.
Stick Slip TechTalkI often hear about how a customer tried using plain bearings for a linear application, but experienced binding or irregular motion. With a little education, this is easy to avoid.
ZLW Belt Actuators by igus®I often hear about how a customer tried using plain bearings for a linear application, but experienced binding or irregular motion. With a little education, this is easy to avoid.
5 Installation Tips for Grease-Free Sliding Linear BearingsLinear rails typically come in lengths between six and 12 feet, but customers often ask: is it possible to make rails longer by butting them together? The answer is yes.
Butting Rails Together in 5 Easy StepsTen years ago, round-shaped ball bearings or T-shaped linear profile rails were the two geometries found on most machines. Nowadays, the introduction of flexible, long-lasting drylin® W linear guides has changed all that.
5 Ways to Choose the Best Linear Guide for Your Application from the drylin® W ToolkitDiscover differences between common types of lead screw technology, such as wear rate, explore a range of lead screw nut options, and more.
Convert Rotary to Linear MotionLinear plain bearings are becoming commonplace in today’s manufacturing industry. As technologies and material sciences have advanced, so have the capabilities of linear plain bearings, particularly those made of plastic, such as the drylin® series of self-lubricating linear bearings from igus®.
Download WhitepaperWhen using drylin® linear guides, it is important to ensure that all acting forces follow the 2:1 rule.
The 2:1 Rule and How to Define Fixed and Floating BearingsA quick-start reference guide to help you select the best linear bearing for your application.
Choosing a Linear Bearing: A Quick Reference GuideOver and over again, the main reasons cited as the causes of bearing failures are lubrication-related issues.
The True Cost of Linear Bearing LubricationCase study about packaging equipment, which has implemented linear bearings that must operate 24/7.
Oil-Free Bearings Withstand 43,200 Cycles 24/7drylin® WJRM - a cost-effective linear bearing that both rolls and slides - for manual applications subject to heavy loads.
How to Lower Driving Force and Friction with Hybrid BearingsWhether you want to design your own linear slide table system or buy one as a ready-made assembly, there are a wide variety of linear products available on the market today.
3 Tips for Choosing a Linear Slide TableA few years ago, we replaced ball bearings on the welding jaw of a vertical-form-fill-seal machine, translating into an impressive 20% increase in throughput.
How to Increase Speeds and Accelerations Using Plastic BearingsI’m sure you’ve heard the saying, “The proof is in the pudding.” But when it comes to self-lubricating plastic bearings, the proof is definitely in the plastic.
The Proof is in the Plasticcable carriers
Cable carriers guide and protect cables and hoses on moving machinery.
Caring for CablesNowadays, plastic cable carriers can achieve almost anything steel can!
Plastic Versus Steel Cable CarriersThere are two key reasons why specialized cable carriers should be used in ESD applications.
The Basics Behind ESD Applications Using Cable CarriersOver the years, cable carriers have increasingly pushed the envelope in terms of higher speeds, longer distances and heavier loads.
Gliding Long Travel Cable Carrier ApplicationsCorrectly arranging every cable and hose within a cable carrier according to the recommended spacing requirements is vital if you want to prolong the service life of your system.
The Cable Distribution Rules You Need to ObeyAccessories - or lack thereof - are a vital part of the performance of a cable carrier system.
Accessorize Your Cable CarrierWhen specifying a cable management system, there are different ways to maximize the service life of your cables. One crucial factor is choosing the right bend radius for the cable carrier.
How to Select the Bend Radius of a Cable CarrierTests prove energy consumption can be reduced by using the right cable carrier material.
Reduce Energy Consumption With Plastic Cable CarriersHere are three different types of rotary applications and the cable carrier system used for each.
A How-To Guide For Rotary ApplicationsContinuous-flex cables
An explanation of the bundling versus layering technique in the construction of continuous-flex cables.
Continuous-flex Cable ConstructionIt's very important for cables used in continuous-flex applications to follow certain construction and performance guidelines.
6 Common Cable Failure ModesSeven common cable management mistakes and how you can avoid making them.
7 cable management mistakes you don't know you're makingThe complex movements made by six-axis robots require special consideration when integrating cables and hoses.
Robotic Cable Management Made EasyConstruction and performance guidelines for cables used in continuous-flex applications.
7 Guidelines for Continuous-flex CablesNew and exciting applications inevitably bring a new set of cabling challenges especially in industrial applications where reliability and mean time between failure are critical.
What to Look for When Specifying a Robot CableAs industrial robotic applications become more and more demanding, flexible cables need to handle more complex movements and still deliver a long service life.
The Less-is-More Approach to Robotic Cable ManagementManaging cables and hoses may seem simple, but in reality it is an important part to of any well-functioning robot.
3 Ways to Avoid Corkscrewed CablesWhat characteristics a cable must have in order to prevent corkscrewing.
Where to Use Cost-effective Continuous-flex CablesIn applications where a low to medium-duty continuous-flex cable can be used, there are some cost-effective options.
7 Guidelines for Cable Installationigus® does not recommend that cables be “relaxed” or “shaken out” prior to being installed into a cable carrier
7 Guidelines for Cable InstallationRevised NFPA 79 standard permits the use of certain AWM cables, many of which can be used for high-flex applications.
plastic bushings
slewing rings
spherical bearings
plastic ball bearings