Change Language :
... functional extension ...
The new firmware update of the D1 includes 11 updates. In addition to the "Modulo axis", which enables time- and path-optimised movements, there is also the "E-cylinder" function, which allows for an easy replacement of pneumatic drives. Further firmware updates, such as "pulse/direction function" with automatic step resolution to minimise noise, CANopen optimisation for information messages or heartbeat function, have also been integrated. You will also be able to install further firmware updates on the D1 in future. We look forward to customer ideas and requests, which we can integrate.
The D1 was developed eight years ago with digital signal processors and an integrated web server interface, so that it would still be up-to-date years later. This basis allows for regular release updates with new features that work with Google Chrome, Microsoft Edge and Mozilla.
Discover more exciting news from the drylin® area