Change Language :
The isense CF.Q module is used for the early detection of the change in electrical specifications of chainflex® cables due to the mechanical loads during operation in an igus® e-chain system®. For this purpose, the electrical resistance of a dedicated conductor loop is measured during operation. Temperature-related resistance changes are compensated for by means of PT100 measurement at the installation location of the cable. Microprocessor-based, continuous data evaluation is carried out by own algorithms of igus®. These form arithmetic as well as sliding average values of the measured resistance values approx. 50 times per second and evaluate them in a temporal context.
If the system detects a permanent change in the electrical specifications, it recommends replacing the cable as soon as possible by switching a potential-free contact. If the cable is not replaced, the system switches off the system as a precaution in the event of a complete core rupture. For later investigations, the system logs all measured values that led to the warning and shutdown.