When new terminals are being planned, stationary SPOs need to be considered at an early stage. As the extended cable length of the cable guidance system on board ships is restricted to 115-180 ft, a stationary SPO has to be installed every 98-164 ft. For a terminal of approx. 1,312 ft in length, this means that 8-15 SPOs have to be installed.
All SPOs have to be connected to switchgear in the distribution station. The costs are immense. Connecting the cables (6.7 lbs/ft) that come from the ship involves a huge amount of work for the port personnel. Several people are needed to handle the cables.
An alternative solution is a shore power supply system with mobile SPOs. With the igus® e-chain® technology for long travels, distances of up to 2,625 ft can be covered. The combination of shore power supply and power & data supply for the STS cranes offers further potential for savings.