To meet the customer's demands and all other challenges, 3 undefined i.Sense undefined (push/pull force detection on e-chains®), i. Sense undefined(tensile force monitoring on cables) and i. Sense undefined (breakage detection on e-chains) are installed.
Second, a undefined is installed. All systems are coordinated with one another and delivered and installed as a package.
Advantages of condition monitoring:
- In the event of an incident with an energy chain, be it a bent guide trough, foreign bodies in the guide trough, a blockage or the breakage of a chain link, the crane operator is informed of the incident and, if desired, the system can also be stopped at once.
The advantages of predictive maintenance:
- Incorporates the functions of condition monitoring and sends a
- Signal regarding maintenance information or replacement of the e-chain®
- All sensor data can be viewed online or in the company network via a dashboard in real time
- Retrievable from different end devices/output channels
- It is possible to set alarms and to respond to increasing force values on the e-chain® or cables and to plan a maintenance intervention on time.
- Values such as temperature, acceleration, speed can be called up in real time via the dashboard