Change Language :
Material | Therman Conductivity [W/m x k] |
---|---|
Steel | 46 |
Aluminium | 204 |
Cast iron | 58 |
V2A | 16 |
Ceramic | 1,4 |
Plastic | 0,24 |
For plastic bushings, the product is given a new value depending on the specific load (p) and the surface speed (v). The p x v value can be considered a measure of the frictional heat and can be used as an analytical tool to answer questions concerning the proper application of a plastic bushing. For this purpose, the actual p x v value is a function of the shaft material of the ambient temperature and the operating time.
Present is:
The tolerated p x v value can be increased in intermittent operation if the plastic bushing temperature never reaches its maximum limit because of the short operating times. Tests have shown that this is true for operating times below 10 minutes. An important qualifier here is the ratio of the operating time and pause intervals. Long pauses make a greater contribution to re-cooling.
The different curves in Figure 1.9 represent different ratios ("3 times" means that the pause lasts 3 times longer than the operating time).
Formula:
Lubrication | Correction factor |
---|---|
Dry operation | 1 |
In the installation | 1.3 |
Persistent, fat | 2 |
Persistent, water | 4 |
Persistent, oil | 5 |