Change Language :
Installation
iglide® plastic bushings are designed to be press-fit, which means they are manufactured oversized as standard. The inner diameter adjusts only after being pressfit into the proper housing bore with the recommended tolerance. The before-pressfit oversized dimension can be up to 2% of the inner diameter, which ensures a proper pressfit. Axial or radial shifts in the housing are also prevented.
The housing bore should be finished in the recommended tolerance and be smooth, flat, and chamfered as far as possible.
Installation should be completed using an arbor press. This is the most efficient installation method and extremely important for preserving the integrity of the bearing. For example, if you use a hammer, the installation of the bearing might be uneven.
Adhesion
Adhering the bushings is not normally necessary. If the pressfit of the bearing could be lost because of high temperatures, the use of a plastic bushing with high temperature resistance is recommended.
If, however, you plan on securing the bushing using adhesives, testing is necessary. The transfer of successful results from other applications is not possible without additional data.
Useful link