Change Language :
Slumping expressly permitted! This is the feature of this high-quality office chair from Nowy Styl GmbH, designed by the famous French architect, Françoise-Hélène Jourda. A healthy and stable spine is supported by the constant switch-over between the hollow and round back. Four patents are responsible for the exceptional seating comfort. Cost-efficient, self-lubricant and maintenance-free iglide® polymer plain bearings from igus® provide for the various settings for the absolutely essential smooth running.
The powerful plastic plain bearings show their strength in the patented "Glide-Tec+" movement kinematics. The lordosis-kyphosis adaptation, a kind of artificial spinal column, is the special highlight of the chair. Movable plastic elements rest on two bent metal rods, which rotate as soon as the user leans back. Thereby the support elements are bent in such a way that the shape of the backrest fit exactly to each sitting position. It is one of the most flexible backrests in the world.
The rotary motion is implemented by plain bearings with flange made of the material with versatile use iglide® J. In this application with a hard chrome shaft, it is distinguished by maximum wear resistance and freedom from noise. Due to the necessary tolerance compensation and for reliably supporting the smooth running, to compensate for possible clearance and to achieve the required low noise, the plain bearings are pretensioned. "Squeaking, creaking or jerking should never occur in a chair of this price segment," says head of design, Franz Eckert.
The plain bearings in the office chair are designed for a weight of up to 440 pounds. Once the user sits down, the automatic weight measurement takes place. When this high pressure load occurs, the iglide® G material displays its strength. It is an economical universal bearing with flange, which is available from stock in more than 650 dimensions. The main design advantage in this application is that it continuously withstands high loads structurally without getting damaged.
Brief portrait: All about chairs
The Nowy Styl Group is a leading manufacturer of office equipment and innovative seating solutions in Europe. The group employs more than 5,500 people and manufactures over 600,000 chairs per month. The German subsidiary based in the Upper Palatinate Ebermannsdorf brings under one roof the expertise of the brands Grammer Office, Forum Seating, Nowystyl and BNOffice Solution. The development of ergonomic seating techniques is the core competence of the Grammer Office brand. The company relies on working closely with the research division to implement solutions that are on the cutting edge of technology and ergonomics. People should sit comfortably in the office and can move naturally at any time, without being restricted by technology. Under the NOWY STYL brand, the company offers a wide range of chairs with the ideal price-performance ratio.
The BN OFFICE SOLUTION brand focuses on office furniture: modular, trendy and smart solutions. A large selection of soft seating and lounge furniture is also sold under the brand name.
The ROHDE & GRAHL brand is known worldwide for its Duo-back concept. In addition to ergonomic office chairs, the company continues to stand for high quality office furniture and customization.
FORUM SEATING is a service provider of professional designing of seating in cinemas, theaters, conference and lecture halls and sports halls and stadiums. Here you can find the right seating arrangement for the most demanding audiences.