- What was needed? Bidirectionally compatible ball bearings
- Requirements: reduced friction, dry-running, maintenance-free
- Material: xirodur B180
- Branch of industry: medical equipment
- Success for the customer: the non-magnetic polymer ball bearings with glass balls by igus are ideal for magnetic resonance imaging and are valued due to their perfect bidirectional compatibility
The rehabilitation system of the Sabancı University in Turkey:
This system is designed as a rehabilitation device to be applied during functional magnetic resonance imaging (fMRI). MRI-compatible rehabilitation devices can be used in the strong magnetic field of MRI equipment for realising physiotherapeutic exercises. This enables the MRI device to display the activated brain regions, leading to conclusions for directing the physiotherapy in such a way that the treatment effectiveness is increased. This can result in positive effects on the quality of life of millions of people who suffer from neurological disorders, such as a stroke.
The device is capable of successfully transmitting controlled forces, measured by fibre optic encoders that are attached to flexible elements. The patients are optimally supported, and at the same time, their safety is guaranteed. This architecture for elastic force control, which achieves excellent force control performance within the required frequency ranges, basically turns the problem of force measurement into a problem of position detection. This force measurement is necessary due to the inevitable friction caused by the Bowden cables.