Change Language :
Configure & calculate lifetime of bearings – current extension with new sizes and products
Easily calculate and configure the service life of your desired linear guide with only a few clicks. Select a drylin® system and add the relevant environmental parameters. Then select the bearing size, carriage, number and position. You then add the distance between the rails and the installation method. Define the coordinates for the drive location and the center of gravity by clicking and dragging the colored crosshair, or enter these via the keyboard. Define the weight, acceleration, and distance of the bearing and select a rail length. The results are displayed.