Change Language :
The products of Motion Solutions GmbH – electric wheelchairs and rehabilitation therapy systems – are all about the mobility of the people who use them. The products themselves are also extremely mobile – for example, the active seating system for wheelchairs, which can be adjusted in various directions, or the heavy-duty wheelchair for people weighing up to 350kg. In the construction of these devices, the designers use our construction kit of maintenance-free plain bearings.
A new development of Motion Solutions is an active seat module, which is installed in existing wheelchairs and provides an astonishingly high degree of mobility: the user can bring the backrest and seat into the overhead position. However, the seat can also be tilted forward in the other direction by up to 33 degrees as a standing-up aid. In addition, the entire seat can be inclined to either side by 20 degrees. Since the movements can be superimposed, the user ultimately sits as if on a large ball, which keeps the body secure in every position.
This is by no means just a gimmick, but supports the health of the physically handicapped. A healthy person, who sits, always shifts his position. This is often not possible for an electric chair user . The possible consequences are circulatory disorders or even open pressure points. With the seat module, the user can shift position and specifically promote blood circulation or simply transfer by standing. All the angles of the seat system can be programmed in such a way that one side and then the other, is pressure-relieved automatically and alternately.
Here, too, the mobility of the user is supported - with extremely movable drive systems. The shears of the cardan system, which are protected by a pair of bellows, are equipped with our undefined. And the designers of Motion Solutions not only use the plain bearing modular system but also the system components of the second business division of igus: our undefined are also used for the energy supply to the movable and adjustable components of the electric chairs.