Change Language :
Carecos Kosmetik GmbH faced the following problem: if a product had to be changed, the company had to have new grippers made for the packaging machines, which would grip the lids and screw them onto cans. The company had previously opted for elaborate machining of grippers made from aluminum. Not only did that cost up to 10,000 euros per part, it also took six weeks. That is too long a wait in an industrial sector, where at the beginning of the era of the Internet of Things it is increasingly important to be able to economically produce even small batches.
Almost every element of a gripper is flexible and glides in its movement on surfaces and shafts and pins, so that the individual parts are exposed to constant wear. Metal parts must often be fitted with separate bearings or lubricated in the application. The use of iglide I150 in 3D printing enabled the company to save up to 85% of the cost and 70% of the manufacturing time compared to the previously selected aluminum formats. Plastic grippers are seven times lighter than metal grippers. In addition to iglide I150, igus® offers five other filaments for the printing of wearing parts in a wide variety of application scenarios. These are up to 50 times more wear-resistant compared to standard materials such as polylactide (PLA) and can be processed on all standard 3D printers.