The French company Arcora has developed a sun protection façade system using a shape memory alloy. When the alloy heats up, the system is able to set a translation carriage in motion. This carriage transmits the force to the rotating sun protection slats via small connecting rods. This compact system makes it possible to replace standard motorizations in building façades, which are more prone to maintenance and repair, noisier and more susceptible to heat.
For the interfaces between the moving (rotation, translation) and fixed elements, the designers were looking for suitable bearings that could withstand dust, weather influences (in a double-skin façade, the temperature can reach up to 158°F in summer) and humidity fluctuations.