Change Language :
Expansion of the chainflex® measuring system cable range CF211 to the larger portfolio for dry environments.
The new chainflex CF211.030 energy chain measuring system cable has been specifically developed and tested for connection to the SIEMENS SINAMICS V90 system. The system presented by Siemens is typically used in the beverage, packaging, textile and solar industries.
igus offers a solution with the best customer benefits with CF211.030. In all of these areas of application, there is no high exposure to oils or cooling lubricants, for example. Therefore CF211.030 with a highly abrasion-resistant and flexible PVC outer jacket is exactly the right answer for all chain applications. We can supply the measuring system by the foot as well as close the gap for the entire V90 system: in addition to the pure measuring system cable sold by the foot, we also offer the motor cable by the foot, and also offer everything harnessed ready for connection. Hence, we have all the products for the system in our catalogue and can deliver them from stock.