The chainflex® CF98 control cable is used by an international electronics company on its eight automated stacking units for phosphorous screens. The previous control cable caused the machines to fail several times. The travel here is just 3.3 feet (1 meter) with 300,000 cycles per month. The space for the unit is extremely small, with a bending radius of just 0.70 inches (18 mm).
Previously, the unit had to be shut down several times to replace cables and the cost of these accumulated downtimes amounted to around $9,300, which was potentially $11,600 per year. This was an untenable situation. Since the installation of chainflex® CF98, there has been no downtime due to cable failure. The control cable increases the long-term operational safety and lowers costs.