Cable Reel Systems vs. energy chain® Cable Carriers


The main differences between cable reel systems & e-chain® cable carriers:

Cable Reel Systems

holding
  • Replacing or adding cables in a cable reel system is a difficult process that causes a lengthy period of downtime.
  • Typical cable reel systems can only manage power and control cables and require special systems for additional cable types, i.e. fiber optics.

igus® e-chain® systems

holding
  • Replacing and adding cables to an e-chain system® is quick and easy as they are always in a safe and accessible position.
  • With e-chain® all types of cables and hoses can be guided in the same system.

holding
  • Motorized reels can require more than 20 feet of space to operate.
  • Cable reels have parts that need to be serviced regularly, which can require a crane and specialized training, as well as significant component lead times and costs.
  • The composite cable used on a cable reel is not protected throughout the length of travel and can be cut or otherwise damaged in the trench or guide system.
igus cable reel
  • energy chain systems® require only a small vertical window for the cable loop (less than 3 feet is needed).
  • e-chain systems® are virtually maintenance free and can easily be serviced without special equipment, tools or training.
  • Cables and hoses are protected within the energy chain in their own compartment for the entire length of travel, which eliminates the risk of cable failure.

motor for drive system
  • Many large cable reels require a motorized drive system to accomplish retraction, which adds to the complexity and maintenance of the system.
  • In traditional cable reels there is constant tension on the cables which can result in cable failure.
holding
  • With e-chain® no additional drives and controls are required, as the e-chain® is pushed and pulled by the machine tow arm.
  • When using an e-chain system® there is no added stress on the cables, push pull forces are handled by the e-chain®.

Contact an Installation and Inspection Services Expert