Change Language :
Successful driving through the winding Danish roads
Conclusion: The filling and the long travel in a confined space make high demands on the energy chains, which are completely covered with cables. The meticulous designing during the run-up was worth it. The first trip of the flatbed semitrailer concluded without any problems. A Danish heavy transport specialist now transported 180 ft long rotor blades from the factory to the port, from where the blades were shipped. Bends and roundabouts were no major challenges for the vehicle. "In my view, there is no economic and/or technical alternative to the energy supply system in this vehicle," summarizes Chief Designer Herbert Swoboda. "Our space availability is more than limited. For us, every single millimeter counts. Nonetheless the holding times should be right, as failure leads to very expensive repairs. And it has to be avoided in any case. “
Go to applied products here
Energy supply systems for extendable heavy load transporter
Operating conditions for energy supply systems cannot be more difficult: Extremely limited installation space, long travel and very high friction coefficients. Furthermore, the filling is extremely difficult. The holding times should also be agreeable with all that, or else high repair costs will accrue. Why the rugged energy chains are technically and economically the first choice in the construction of an extendable heavy load transporter is shown in the following article.
"When extending the vehicle, the energy supply system is exposed to very strong push-pull forces, which they must simply endure in the long term. " The company Goldhofer with about 650 employees today has a history of more than 300 years. Started in 1705 as a forge, it has dedicated itself to intelligent solutions for the road, heavy goods and special transportation. The product range includes trailers, semitrailers, heavy goods transport systems and aircraft tugs. The specialist for heavy loads has already delivered more than 33,000 heavy-duty trucks and heavy load vehicles in over 70 countries worldwide.
energy chains in the innermost tube
In the development of the triple-telescopic platform, the extremely rugged energy supply systems were the first choice.
The technical requirements are extremely high. Above all, in the present application there is a safe rolling of the heavy supply cables in the telescope. The telescope system consists of four rectangular tubes. The energy supply lines run in minimum space in the innermost tube. Only a width of 340 mm and a height of 577 mm are available as installation space. Every millimeter counts here.
"For this reason we need to rely on the functioning and stability of the energy chain under all circumstances. " A further complication is that other forces may act on the energy supply system. "A tube can, for example, buckle while pulling put, so that the chain has to withstand jerky movements in the short term. " In addition the high temperature fluctuations in the tube - from -13°F to + 122°F depending on the season - also play a role.
More applications from different sectors