Change Language :
Roller-style cable carriers in a compost plant
Heat, abrasive dirt, high humidity: these are just some of the ambient conditions in a compost plant. Every single component is called upon to last a long time and avert unnecessary machine downtime. In this application, roller-style cable carriers have been in successful operation for the past 2 years.
Since the compost plant opened, various different igus® cable carriers have been operating in the ‘layer-rearranging unit’. Whereas before the plant manufacturer recommended an urgent replacement every year, since the time roller cable carrier systems – so-called ‘Rol-E Chains® from igus®’ modular, rugged E4/4 System - were installed, a minimum lifetime of five years can be expected.
The application conditions in the compost plant influence not only the cable carriers, but also the cables responsible for the energy supply. If they become brittle and corkscrewing occurs, the main supply line could go down and the entire plant would come to a standstill. For this reason, the plant procures continuous-flex cables from igus® and has done since 1999.
‘chainflex® CF 5' unshielded control cables are used onsite. This cable series’ structure - with its gusset-filling pressure extruded inner jacket and PVC outer jacket – means it is suitable for heavy-duty use.
The factory manager confirmed that service life has been increased as a result of using energy chain cable carriers and chainflex® continuous-flex cables.