The linear drive in the x-direction is provided by a linear robot combination of two stepper motors which drive two trapezoidal lead screws. These are flange-mounted using lead screw bearing blocks from igus. Using plastic lead screw nuts made of iglidur J, which are mounted on two drylin T guide carriages on each side, the rotational movement of the trapezoidal lead screw is converted into a linear movement. This design ensures the movement of the y-axis. The device for infeed in z-direction in the working area is installed on this transverse axis. Shaft end support and infeed are each moved by a trapezoidal lead screw, four guide carriages (drylin T), which move on guide systems, and a stepper motor. By installing the appropriate tools, this linear robot is able to carry out light milling operations, measuring operations and 3D printing.
The majority of all components such as lead screw bearings, nut holders,