Change Language :
Conventional skate wheel guides in particular often have both mechanical and economic disadvantages in linear actuators. For example, their stiffness is very poor. They are susceptible to high moment loads and allow only limited acceleration. In addition, there is usually time-consuming and cost-intensive maintenance work. Guide systems with plastic elements put an end to these problems and open up many more advantages for the user.
For cost-conscious design
All igus guides are particularly characterised by simple design, robustness and compact construction, design focus for the entire "LCB". This results in a low moving dead mass due to the glide pads and the slim runner plate as well as a wide guide base in close proximity to the load. Speeds can reach up to 8 m/s; unrestricted acceleration is possible. Last but not least, the actuator has a high level of resistance to chemicals and corrosion. Perhaps the most important plus point of guide systems, however, is their cost-effectiveness.
On the one hand, this is due to the favourable purchase price, and on the other hand to the minimal operating costs, as drylin works maintenance-free even in harsh environments. Since there is no need for lubrication, the guide does not attract dirt and does not contaminate the overall system by leaking grease or oil. Expensive machine downtimes are a thing of the past. Additional protection or scrapers are also unnecessary, which reduces the number of components to be mounted and further lowers costs. Lindemann: "For our skate wheel guides, at least twelve skate wheels have to be pre-assembled, mounted and adjusted, whereas for the guide system, only four sliders. The working time alone for assembling the guide system is reduced to an estimated 10 per cent." When the wear limit is reached, the user can simply change the glide pads himself within a few minutes. Even pneumatic and servo-pneumatic solutions can be advantageously replaced, according to Lindemann, whereby the better positionability at any point is also decisive here: "Actuators with linear guide systems can even make some designs with linear motors look pale, if it is not so much a matter of accuracy, but rather the lower energy consumption for oscillating movements that is important. This is due to the much lower movable dead masses."