Change Language :
Dercks Gartenbau GmbH designed the precision watering trolley with the aim of conserving groundwater resources and saving energy costs. Following a successful first prototype, the second model with a 45m span has now been constructed for the targeted irrigation of potted plants over 9,190m2 of area. To ensure that the supply cables and the two hoses for the water supply are not pulled over the ground, they run safely over the ground in an energy chain. Together with intelligent sensors for measuring push/pull forces, a reliable energy supply system was implemented.
"The energy chain is a must in order to achieve the maximum use of space on the floor space of the precision watering trolley. With the additional floor space gained, the investment in the energy chain pays off in four years. We are therefore happy to be able to use the energy chain here."
Peter Dercks, Dercks Gardening GmbH
Tech up ... Cost down
This awards booklet contains real life examples of how customers have improved technology and saved money using energy chain systems for cable management.