3 Methods for Installing a Cable Carrier Vertically

Vertical Standing Cable Carriers

verticle cable carrier
  1. Consult with a sales engineer who can assist with all combined aspects of your application, including the load, stroke height, bend radii, and cable carrier type.
  2. If a cost-saving solution is required, contact igus® to inquire about combining horizontal and vertical movements.

Vertical Hanging Cable Carriers

cable carriers lateral acceleration
cable carriers lateral acceleration

Camber

hanging cable carriers
hanging cable carriers
  1. Using mounting brackets will increase the performance of a cable carrier system. When working in restricted spaces, it may be beneficial to consult a sales engineer for other possible solutions.
  2. Safe strain relief and clear separation of the cables are absolutely critical. Remember: cables must be able to move freely, and bear the entirety of their own weight in a hanging application!

Zig-zag Cable Carriers

zig-zag cable carrier
  1. The use of pivoting mounting brackets is recommended with a zig-zag style installation. With these types ofbrackets, a pivoting connection exists between the mounting bracket and the first chain link in order to relive pushforces on the chain link.
  2. It is recommended to always consult with a sales engineer when considering a zig-zag style cable carrier installation. Different application factors can greatly affect the maximum speed and acceleration of this type of installation.

Looking to Speak with an Expert?