Example 3: tested, tested, tested! "Millions of cycles" in a cable carrier

Sliding application as the basis of the test structure

 

Profibus cables in continuous-flex industrial applications

Competition between cable suppliers is intensifying and manufacturers constantly try and outshine each another with promises to “guarantee service life for cables used in cable carriers”. Catalogs claim 10 million - or even as many as 50 million - cycles when it comes to the service life of cables in moving applications.

On taking a closer look at the figures, you have to ask ask how testing was done, or how realistic the tests carried out actually were (for example the length of travel, test radii, etc.) in order to be able to provide such a guarantee. Even information stating that cables are tested in accordance with VDE (Association of German electrical engineers) 0472, Part 603, test method H, is not helpful when it comes to determining the service life of a cable in a cable carrier, since there is no special VDE test for this.

Differences in service life

At the beginning of 2002, a test to determine the service life of profibus cables in a real-world application was commissioned by igus’ test laboratory. The aim was to examine any differences in the service life of igus®’ CFBUS.001 Chainflex® cable and another market-leading profibus cable. The parameters required for the test were selected on the basis of data contained in the competitor’s catalog:


Catalog details Test item “A”
Twin-core
profibus cable
Test item “B”
igus® Chainflex®
CFBUS.001
 
Cross section (2 x AWG24)C (2 x 0.01 inch2)C
Guaranteed lifetime Min. 4 million cycles To be determined in
a test
Bending radius > = 2.36 inches 3.35 inches
Diameter 0.31 inches 0.33 inches
Catalog details as in 2002 as in 2002

Test parameters according to catalog data of the competition

A gliding application was chosen as a suitable test structure since profibus cables are usually used here because of their data integrity, particularly over long lengths of travel and long transmission distances.

In order to be able to carry out non-destructive testing and achieve a large number of bending cycles in a short period of time, a genuine profibus transmission path was constructed. In a PC at the fixed end of the test cable carrier there was a profibus master-insert card. A connection to a profibus slave was located on the moving end. This enabled the transmission rate to be determined with the help of a diagnosis program. Any data packets which might have been transmitted incorrectly could be indicated. The highest-possible transmission rate of 12 megabits/s was tthereby set.

The fundamental test, which began at the beginning of 2002 and is still in progress today, showed only a relatively low number of cycles (420,000) resulted in the total failure of test item “A“, which - according to the competitor’s catalog - should have functioned safely for at least 4 million cycles. The actual service life achieved deviates from that indicated in the catalog by a factor of ten.

On the other hand test item “B“, the CFBUS.001, is still undergoing testing without any problems in data transmissions. So far, it has accomplished more than 14 million cycles.

Structure and materials

The main reason for the major differences in service life is the differing structural parameters of test item “A“ and test item “B“ (CFBUS.001), as well as the different materials used for producing the cables. The conductor insulation of the bus is comprised of a foam material for all the test items. The electrical assets of this material ensured better transmission properties. A disadvantage of this material was its weakness under reverse stresses. The forces which affect the bus pair should be absorbed by the element sheathing in order to alleviate the mechanical stress of the conductor insulation.

Highly-elastic element sheathing

For this reason, test item “B“ (igus®) was provided with a mechanically-superior, extruded-TPE inner sheathing to fill any gaps and to protect the bus pair against mechanical influences during the bending process. The element sheathing needs to be highly elastic. A mechanically-inferior element sheathing made of inexpensive filling material only serves to make the bus pair round and is not able to protect the bus cable from the high degree of mechanical stress present inside a cable carrier. Tensile and compressive forces which occur mainly influence those parts of the cable core in which there is a break in the element sheathing.


Test parameters  
 
Distance of travel: S = 16.41 ft
Speed, approx: V = 11.48 ft/s
Acceleration, approx.: a = 24.61 ft/s2
Radius, approx.: 2.16 inches


The sheathing of test item ”B“ (CFBUS.001) is characterized by a mechanically superior, gusset-filled TPE jacket, which mechanically relieves the bus pair, fixes the cores in a defined position and is flexible. The extremely short pitch of the core strands and continuous-flex cable also ensure that no great tensile or compressive force has an effect on a long length of core.

Number of cycles tested  
Broken element jacket

A mechanically low-quality element jacket can’t protect the bus pair against the high mechanical loads inside a cable carrier.

 

UL and CSA approval

Chainflex® CFBUS cables are now also available for all standard field bus systems, complete with UL and CSA approval and DESINA compliance. The highly abrasion-resistant, flame-retardant, TPE outer jacket is extruded onto the fully braided shield with an adjusted twisted angle in order to provide the cable with additional stability.

The bus elements braided with a particularly short strand pitch are protected by means of a gap-filling, extruded TPE inner jacket. The bus parameters required are fulfilled by means of a choice of coordinated insulating materials and production procedures.

As with all Chainflex® cables, the new standard field bus cables of the CFBUS series are now available ex-stock, without any cutting costs or extra charges for small quantities.

More information
igus® inc.
PO Box 14349
East Providence
R.I. 02914

For immediate assistance in North America:
Call 1 (800) 521 2747

E-mail us

Subscribe to
e-newsletter
Contacts in your location (can be on-site within 24-48 hours)

myigus myCatalog
No minimum order
On-site and telephone support Delivery from 24h* Free samples

About Chainflex®Product OverviewProduct SelectorLifetime calculationPinout ConfiguratorPart No. searchRequest a quoteCatalog/sample requestEmail the product expertApplication examplesVideosTechTalk Design Advice SeriesDownloads

More than 100,000 products available! Open Mon-Fri 8:00 am - 8:00 pm EST.
No minimum order

Terms and Conditions Imprint General Information Data Privacy Protection Declaration