Plastic fiber-optic cables are used for data transmission in industrial applications due to their excellent resistance against electro-magnetic fields, their small size and low weight. However, operating as a continuous-flex cable inside a cable carrier places high demands on these cables.
The most important properties of a fiber-optic cable relate to 'dispersion' and 'attenuation'. Dispersion is the spreading of the signal in time. In plastic fiber-optic cables this involves ‘modal dispersion’: the spreading of the signal in time resulting from the different propagation modes in the fiber. Dispersion determines important transmission properties, such as bandwidth, cut-off frequency or maximum bit rate. Significant changes in dispersion could not be determined in any of the tests carried out, so it can be concluded that the industrial application of igus® Chainflex® fiber-optic cables inside cable carriers is unproblematic in terms of dispersion changes.
Attenuation determines the maximum possible length of a transmission path. The attenuation of a plastic fiber, such as a glass fiber, is also strongly dependent on the wavelength of the light used. For this reason, all the tests were carried out with a wavelength of 666nm.
Depending on the output of the transmitter and the sensitivity of the receiver, the operator has an attenuation budget available for the complete transmission path - including all junction and transition regions. This attenuation budget (typically approx. 20dB) must not be exceeded if a secure data transmission is needed. To know whether and to what extent increases in attenuation are to be expected for a particular application is important so these can be taken into account for the compilation of the user's own attenuation budget.
In addition to continuous bending stress, further mechanical stresses that can occur during installation or operation must be taken into account. For example, relatively large tensile forces can occur when integrating the cable into a cable carrier. Fixing the cables at the ends of the cable carrier using cable clamps also leads to permanent transverse loads. To analyze the behavior under transverse loads, tests were carried out according to DIN VDE 0472, Part 223. Since the cable clamps only exercise pressure in an area covering a few inches, increases in attenuation are relatively low. Attenuation under tensile loads depends to a great extent on the composition of the cable. Cables with integrated copper conductors or strain relief elements do not reveal a noticeable increase in attenuation until much greater tensile forces are applied.
Figure 1 represents test results for a Chainflex®-line with 6 fiber-optic cables. The length of the test sample is 1m and the maximum tensile load 250N.
The tensile forces required to integrate fiber-optic cables in Energy Chains® are usually much lower than 250N. The increase in attenuation was 0.17dB at the maximum tensile force and disappeared completely after the tensile load was released. No effect on attenuation should be expected. With continuously-bending plastic fiber-optic cablesm additional factors such as material fatigue, dulling of materials, micro-cracks, and even complete fiber fracture should be considered for their influence on attenuation. This can only be investigated in extensive practical tests, such as those carried out by igus®.
Figure 2: Course of the increase in attenuation as a function of the number of cycles.
Fiber-optic cable tests from other manufacturers have not shown such impressive results - some even failed after complete fiber breakages. In contrast, the igus® tests revealed that Chainflex® fiber-optic cables are not influenced in their function by mechanical loads such as tensile, transverse or bending stresses. They are perfectly suitable for use in – sometimes demanding - industrial environments for the interference-proof transfer of information between drive and control elements of machines.
Subscribe to
e-newsletter
Contacts in your location (can be on-site within 24-48 hours)
About Chainflex®Product OverviewProduct SelectorLifetime calculationPinout ConfiguratorPart No. searchRequest a quoteCatalog/sample requestEmail the product expertApplication examplesVideosTechTalk Design Advice SeriesDownloads
More than 100,000 products available! Open Mon-Fri 8:00 am - 8:00 pm EST.
No minimum order