The "FLG" type of installation always generates the longest service life and can be operated with the maximum values for speed and acceleration.
If the upper run of the Energy Chain® operates without touching the lower run over the entire travel, it is called an unsupported application.
The distance between the cable carrier's moving end and the beginning of its radius' curve is called the Unsupported Length. It is always dependent upon the type of cable carrier and the fill weight.
Example for unsupported straight FLG
The "FLG" type of installation always generates the longest service life and can be operated with the maximum values for speed and acceleration.
FLG unsupported straight length
FLB unsupported length with sag
The "unsupported" application is the most common. igus® Energy Chains® are very well suited for high dynamics and long service life. The maximum unsupported length is dependent upon the fill weight and the type of cable carrier. As a result, we differentiate among three types of unsupported length:
The "FLG" Energy Chain® applies when the upper run either has camber, is straight, or has a maximum of 0.39-1.97 inches (10-50 mm) sag, depending on the size of the cable carrier. The "FLG" type of installation is always preferred. The Energy Chain® runs quietly and is not exposed to any additional vibration.
The "FLB" Energy Chain® applies when the sag amounts to more than 0.39-1.97 inches (10-50 mm), depending on the cable carrier size, and less than a defined maximum sag. This maximum sag is dependent on the type of cable carrier. The "FLB" application is technically permissible in many cases. It becomes problematic if the acceleration and the travel frequency are high.
If the sag is greater than permissible for "FLB", then we refer to it as "critical sag." An installation with critical sag must be avoided or reserved for extreme circumstances. An Energy Chain® should never be installed with critical sag. There are applications which, after a very long period of use, reach the stage of "critical sag." The cable carrier should be replaced at that time. Please contact us if your application reaches critical sag.
Example of unsupported with FLB sag
For every igus® cable carrier, the"FLG" and "FLB" values are essential for:
Finding a suitable Energy Chain® for your fill weight and travel distance
Identifying the maximum load for the selected Energy Chain®
Unsupported Length
Speed
Acceleration
Service life
Load bearing areas
Noise level
Technical environment
If your application, fill weight and travel fall outside the "unsupported length" parameters of the desired Energy Chain®, you have the following options:
Select a more stable Energy Chain®
Support the cable carrier in the unsupported area (this possibility has restrictions for acceleration, speed and noise as a consequence; three fundamental examples are detailed below. Please consult igus® if you are considering this possibility. We will gladly provide you with a detailed proposal.)
Use a "multiband" cable carrier or "nest" two Energy Chains® inside one another. (Please consult igus® regarding these options.)
Design the travel distance as a "gliding application".
Series 28 with support in the FLB area
Support of the FLG area. The overall straight, unsupported travel can be increased along the upper run by a maximum of 50% of the FLG and along the lower run by a maximum of 100%.
Support of the FLB area. The overall travel distance can be extended to a maximum of 100% from FLB.
For unsupported applications, the acceleration (a) is the critical parameter. High acceleration can cause the cable carrier to vibrate and reduce its service life. This is a particular danger if the cable carrier already has a sag greater than the FLG value. Maximum values for acceleration, speed, and service life are achieved only with cable carriers incorporating the FLG design. FLG designed Energy Chain Systems® can sustain very high loads. To date, a peak acceleration of 2,572 feet per second has been achieved during continuous use. Through ongoing testing in the igus® laboratory and from practical experience, standard values for service life have been formulated (see graphs). Our tests confirm that these standard values apply to all igus® Energy Chains® and E-Tubes. It is crucial to determine whether the application will be designed as unsupported straight FLG or unsupported, with sag FLB.
| FL G | FL B | ||
| v max. | ft/s (m/s) | 32.8 (10) | 9.83 (3) |
| v peak | [ft/s] | 65.6 (20) | - |
| a max. | ft/s 2 (m/s2) | 65.6 (20) | 19.69 (6) |
| a peak | ft/s 2 (m/s2) | 2,572 (784) | - |
Standard values on service life for FLG, (unsupported straight), dependent on acceleration
Standard values of service life for FLB, (unsupported sag), dependent on acceleration
Unsupported Energy Chains® normally require some type of surface on which the lower portion of the cable carrier runs. A wide range of configurations is available, as the drawings on the right demonstrates. Many material options are feasible: metals, polymers, stone, wood, concrete, glass, etc. We also have solutions to minimize the noise generated by the cable carrier’s lower portion. Please consult igus®. When selecting the running surface, be sure dirt and debris cannot collect in the cable carrier's path.
Different surfaces and guide troughs are possible
We recommend pivoting mounting brackets as standard for unsupported applications. Pivoting mounting brackets compensate for the camber, can be installed more easily and decrease the load on the first Energy Chain® link in operation. Exception: if the acceleration is greater than 66 ft/s² or if the height is limited to the HF measurement, locking mounting brackets keep the Energy Chain® under the HF measurement.
We recommend pivoting mounting brackets as standard. We recommend locking mounting brackets as standard if high speeds > 217 ft/s (66 m/s) or accelerations > 217 ft/s² (66 m/s²)
Energy Chains® without support along the lower run have restricted use. The value FLU usually must be determined in a test by igus®. The maximum permissible amount of the projection depends on the fill weight, the selected Energy Chain®, the dynamics, and other factors, because the various combinations of these parameters can produce very different results. If the lower run of the Energy Chain® cannot be supported over the whole travel, please consult igus®.
Series 40 Energy Chain® partially unsupported. Please consult igus® regarding this type of configuration.
Subscribe to
e-newsletter
Contacts in your location (can be on-site within 24-48 hours)
About Energy Chains®Product OverviewProduct Selector3D-CAD libraryPart No. searchRequest a quoteCatalog/sample requestEmail the product expertApplication examplesAssembly InstructionsVideosTechTalk Design Advice SeriesDownloads
More than 100,000 products available! Open Mon-Fri 8:00 am - 8:00 pm EST.
No minimum order