Gold vector® 2008: Handling system ”roboLoop“
The ”roboLoop“ system itself offers manyways to optimise the fabrication sequences.

Modern plastic energy chains® are the umbilical cord of the automation, machine and plant engineering industries. These energy chains® ensure the safe supply of energy, data, pulses and operating media and are always in motion. Energy chains® are suitable for multipurpose use in the crane and machine tool industries and in the robotics and clean room industries.
The ”roboLoop“ system itself offers manyways to optimise the fabrication sequences.
The rail & Tracking systems are used whereverfast camera movements are an important factor as, for example, at sport competitions,but also at many popular events such as concerts, stage shows, etc.
This OpenHydro tidal turbine generates electrical power through the inflow and outflow of water.
Theproblem with previous data glove solutionswas that the sensors in the gloveswere subject to extreme loads and thatmovement signals were also producedunintentionally during sideways movements.
This telescope has been installed on theCanary Island of La Palma and registersthe gamma rays that strike the earth fromouter space.
A solution for media elevators previously unavailable in the market has now beenrealised with igus® E-Chain Systems®.
The door systems in this application guaranteethat the temperatures prescribed for the productand storage of perishable products, such asfood, are strictly observed.
Because the intended place ofuse for the energy and the control system is variable and may be situated at a height of10 metres.
This application showed that a vertical stroke of more than one metre and a swivellingrange of 270° can be implemented in the limited installation space of the grinding headin a gear-grinding machine.
TheEnergy Chain® was installed on an injection moulding tool so thatno additional space is necessary in horizontal direction forthe unreeling movement.
In the case of this industrial robot, a rigid pipe between the 3rd and 6th axis wasreplaced by a multidimensional, flexible Triflex® R energy chain®.
Several igus® Energy Chains® are used here, including one mounted vertically with a reverse bend radius.
This drill is used in extremely demanding offshore environments and uses continuous-flex cables from igus®
For this application, aircraft engine parts arewelded together.
This laser distance-measuring telescopeuses four igus® Energy Chains® of the Triflex® R series.
The ”OPTILIGHT“ elevator doors presented here can represent informationsuch as storey numbers on the glass surface areas.
The ”Virtu“ large-format printer can be used to print almost anything: sheetmetal, foils, textiles, wood, glass, and, of course, also paper in widths up3.5 metres.
In the case of these robots, the hosepackage had to be replaced very fewweeks.
This newly developed stern thruster helps sailboats during difficult manoeuvres such as, for example, passages through locks;but because of its high performance, it can also be used as a main drive unit.
The marking unitmoves like a robot about several axes.
Medical students and physicians can practise diverse vascular surgicalinterventions on this device.
Very high accelerations proved an enormous challenge for the design engineers of this robot.
This newly developed gas-fired furnace only requires onethirdof the usual time to heat up rollers in the steel industry
This energy chain® in the palletising system of a dairy is subject toextreme load with more than 5,000 strokes a day.
Crane in a truck assembly plant used to unload and transport individual vehicle chassis at the beginning of the assembly process
To control andsupply the lying surface area, data and electrical cables, including hydraulic hoses, are run along the column.
Sawdust is also not a problem for igus® Energy Chains®.
Almost daily failures of this inclined hoist in the URBIS art centre in the Manchester citycentre have become a thing of the past with the deployment of the igus® Energy Chain®.
This height-adjustable design speaker’sdesk is very flexible in its features.
The igus® Energy Chain® E6 demonstrates its strengths inthe case of this cutting tool.
In the case of this application of a spray-painting robot, the ATEXproperties of the energy supply system are important most of all.
This workpiece storage location is designedfor automated shift operation. At the same time, the energy supply mustbe provided in all four axes of motion(three linear axes and one rotational axis).
In the case of machine tools, thetrend is also going in the directionof compactness.
A multidimensional Triflex® R cable carrier is used here to manage and protect the cables.
To save installation space and toreduce forces and torques, an Energy Chain® was wound around a gripper.
The special feature of thisapplication is the hot chips produced during the machining process, which do not stick tothe igus® Energy Chain® and therefore extremely reduce the maintenance expenditure as a result.
The cable carrier on this drilling machine must withstand extreme vibrations and dirt.
The igus® Energy Chain® B17 was just completely alienated from its intended purpose for this clever application.
In the case of this application, the worksafety was increased by integrating theenergy supply system into the body of thepallet changer.
Visible for approx. only one minute are these pictures, which are ”printed“ with UV lighton a light-sensitive screen.
Until recently, you could not purchase a solution anywhere in the world for this application.
With the perfectly fitting energy supplysystem for this crane system, the overalldimension for the installation was considerablyreduced.
The deployed Energy Chain® ofthe E2 mini family meets all the requirementsand has been in use without anyfailures for more than six years!
Cable carriers and continuous-flex cables for belt-driven automatic gates
After its completion, this giant telescope in Arizona(USA) will look deep into our universe; the two mainmirrors each have diameter of 8.4 metres.
In the case of this adhesive resin system, a lifting platform moves upwardto a height three or four times a day to empty barrels with a volume ofapprox. 200 litres.
Previously, several individual hoses had to be fastened in the energy supplysystem to prevent them from squeezing each other.
Parts can be machined in one go with this new CNC grinding machinebecause it is equipped with two grinding heads on one rotating shaft.
An System E6 Energy Chain® cable carrier speeds up the wafer handling process in this chip production plant.
Measuring and regulating system in the area of blown film extrusion
This portal milling machine is used to manufacture points forrailway networks
Dismantling tool for nuclear power plant decommissioning
This application needed a compact cable management solution that would be wood-chip resistant.
In this application, foodstuffs are weighed for thepreparation of convenience food.
In this paint-spraying machine, sensors aremoved over minimum space.
For some applications that require high electric power, conventional copper cables aretoo heavy.
Subscribe to
e-newsletter
Contacts in your location (can be on-site within 24-48 hours)
About Chainflex®Product OverviewProduct SelectorLifetime calculationPinout ConfiguratorPart No. searchRequest a quoteCatalog/sample requestEmail the product expertApplication examplesVideosTechTalk Design Advice SeriesDownloads
Terms and Conditions Imprint General Information Data Privacy Protection Declaration