| |
|
![]() |
|
| And the winners of the 2005 Mini manus contest are ... | |
|
![]() Solution: The iglide R flange bearings were used because of the direct size interchangeability to the bronze bushings. The iglide bearings were used to eliminate the need for greasing 14 grease points. This decreases the maintenance time required. Secondly, owners do not want grease falling onto the freshly cut grass, for environmental and cosmetic reasons. Using the igus bearings also deliminated the machining costs required for the grease nipples. |
Technical advancement through the use of plastic bearings: Replacement of an existing solution Economic impact of using plastic bearings: Type of bearing: iglide R Application: Problem: |
|
|
Solution: |
Technical advancement through the use of plastic bearings: Replacement of an existing solution Economic impact of using plastic bearings: Type of bearing: Drylin N linear guide system Application: The position of the needle in this assembly is determined by a combination of motor steps and the interrupt switches. The needle is required to move to four different positions during the injection cycle: The upper interrupt switch is used to define the stream position of the needle cross port. The seal position and the vial position are determined by motor steps. There is another position called the “auto-add” position which is used when the needle has been retracted from the vial in-between “auto-add” sample draws. The lower switch is used to determine the position of the needle for the “auto-add” operations. Problem: |
|
|
|
Third Place Bronze manus Award:BC2A Design, Inc. San Jose, Calif. Plastic Bearing: iglide G300 |
![]() |
Technical advancement through the use of plastic bearings: Economic impact of using plastic bearings: Type of bearing: iglide G300 Application: |
|
Problem: Second to function, weight is the primary driver; all components have to be as lightweight as possible, every gram counts in the total weight. Because this is a low volume product, profit margins are inherently low and individual part cost is important. Competitors use steel backed PTFE bearings in this type of application, but under extended use, the thin PTFE lining becomes saturated with road debris, severely limiting the bearings life and functionality. Solution: Working directly with igus representatives we were able to test several different iglide series bearings under varying real-world conditions. The iglide G300 bearing series, with it’s unique combination of low friction, long life, low weight and low cost, answered all of our concerns and is now used in both pivot points in the dual pivot caliper design. The brakes were most recently successfully raced at the San Francisco Grand Prix bike race, billed as “ America ’s Toughest Bike Race”. |
|
| Read the press release announcing the results. | |
History of manus Last year, igus unveiled the first North American Plastic Bearing Design Contest. Contestants from across the United States and Canada competed to win various prizes. Applications ran the gamut from sports equipment, to medical devices and woodworking machinery. Check out manus 2004 |
|
The winning applications from 2004: |
|
Two manus Contests have been held by igus Gmbh in Germany, one earlier this year and the other was the first-ever manus Contest held in 2003. The success of that endeavor led to the North American manus Contest in which more than 60 contestants took part. Igus UK followed up next with its own manus Contest late last year and now igus offices worldwide are planning manus contests as well. Check back for updates on the next manus competition. Congratulations to the winners and to all who participated! Those who didn't win this year are eligible to resubmit their application in any upcoming manus contests. If you have questions or comments, please contact Farrah Phillipo, manus coordinator at (800) 521-2747 or via e-mail at fphillipo@igus.com. |
|